2024-03-18 10:17 AM
I got this assembly code (see below) in an ST example code on secure boot and and I don't understand some lines :
Does anyone have better understanding?
1 .global launch_application
2 aunch_application:
3 /******************************************************
4 * return from exception to application launch function
5 * R0: application vector address
6 * R1: exit function address
7 * push interrupt context R0 R1 R2 R3 R12 LR PC xPSR
8 *******************************************************/
9 MOV R2, #0x01000000 /* xPSR activate Thumb bit */
10 PUSH {R2}
11 MOV R2, #1
12 BIC R1, R1, R2 /* clear least significant bit of exit function */
13 PUSH {R1} /* return address = application entry point */
14 MOV R1, #0 /* clear other context registers */
15 PUSH {R1}
16 PUSH {R1}
17 PUSH {R1}
18 PUSH {R1}
19 PUSH {R1}
20 PUSH {R0} /* R0 = application entry point */
21 MOV LR, #0xFFFFFFF9 /* set LR to return to thread mode with main stack */
22 BX LR /* return from interrupt */
23 .end
2024-03-18 2:13 PM
It is what I'd characterize as a "call gate" it determines how the MCU unstacks the processor context.
Depending on the patterns, it picks one stack or the other, and unwinds the NVIC depth.
Perhaps look a one of Joseph Yiu's Essential Cortex-M books, or ST's Programming Manuals, or the ARM TRM
2024-03-26 2:36 AM
Thanks for the tip, I read Joseph Yiu's book and understood better the call gate mechanism.
I still have a problem with the line 21 :
MOV LR, #0xFFFFFFF9 /* set LR to return to thread mode with main stack */For a reason that I don't understand , #0xFFFFFFF9 is being considered as an address and branching to it is causing the hard fault. See capture attached.
Does any one have a clue why #0xFFFFFFF9 is being considered wrongly as an address?
Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.