STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 Custom HID device, host read callback

Hi,I am new to HID and have some questions regarding the ST HID Middleware package.I am using an STM32F479F as a Custom HID device. I used the example from the STM32 USB training to get everything up and running. It works.When the host (PC) performs ...

IHC by Associate
  • 1235 Views
  • 0 replies
  • 0 kudos

UxDevice_HID_CDC_ACM example

Am trying to Use of a USB to transmit data (transmit/receive) between a board and anHyperTerminal PC application.    Am working with Nucleo-STM32H563 board. But i didnt get expect data in hyper terminal. Here i have attached code part . Kindly correc...

RKOAS by Associate II
  • 1766 Views
  • 2 replies
  • 0 kudos

Issue in downloading SD card data by USB

I am currently working on a project that involves integrating USB functionality for data transfer and data logging on an STM32F407VG micro-controller. Specifically, I want to log data files on an SD card and enable the user to download these logged f...

STM32WLE5CCU6

Dear,I am currently in the process of designing a custom PCB with your STM32WLE5CCU6 chip (QFN Package). Consequently, I have a few questions:Given that the PCB will be exclusively sold in Europe and that I need to optimize power consumption, should ...

NUCLEO-H743ZI ethernet protocol with keil

I want to start the ethernet protocol with NUCLEO-H743ZI. For this I used the following tutorials :https://community.st.com/t5/stm32-mcus/how-to-create-project-for-stm32h7-with-ethernet-and-lwip-stack/ta-p/49308https://github.com/stm32-hotspot/STM32H...

mjadi.1 by Associate
  • 1996 Views
  • 2 replies
  • 0 kudos

DEBUGGER NOT WORKING: STLINK/V2

Hi Team,Recently i was using stm32 stlinkv2 in the STM32F411CEU6. They debugger was workig fine . After flashing 10-20 times , the debugger stopped working and throwig up the error:STMicroelectronics ST-LINK GDB server. Version 7.4.0Copyright (c) 202...

neelimas by Associate II
  • 5154 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.