2020-04-17 9:17 AM
Hello,
I am using nucleo-64 board and CubeIDE in linux ubuntu.
Everything is working fine except I can not see any of my serial output from the application.
St-link is connected to usart2. I thought they could be used at the same time.
Do i need to use a separate serial port for my serial output ?
I tried to connect the nucleo board to my computer via a serial monitor to see the output but the serial terminal connection was unsuccessfull on any of my usual ports /dev/ttyUSB0 or /dev/ttyUSB1 .
Thanks
2020-04-17 9:52 AM
>>St-link is connected to usart2. I thought they could be used at the same time.
The ST-LINK debugger and VCP can work concurrently, issue here with tools, drivers or OS
>>Do i need to use a separate serial port for my serial output ?
You could even use the same UART, and then a USB-to-CMOS Serial dongle that the tools don't interfere with.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.