2020-10-16 7:50 AM
2020-10-19 5:58 AM
In the device manager there should be something visible. Depending on the settings there should be e.g.:
Can you see anything of that?
Regards
/Peter
2023-08-25 8:50 AM
Hello Peter,
I have issues communicating with Nucleo-G431RB using usb driver STSW-LINK009 in win10. Here is what I found. After plugging in the use cable to my laptop, I saw an "unknow USB device (Device description request failed)" showed up in the device manager and with an exclamation mark !. Nothing worked after that. The driver seemed to be installed correctly, because an "USB Mass Storage Device" showed up when I plugged in Nucleo-F103RB board and communication was working normally. Is it because the different between ST-Link/V2-1 vs. STLINK-V3 G431RB had? How do I remedy this issue? Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.