2022-11-11 8:05 PM
1)is crystal is required to be used for program flashing
2) boot0 to be low or High
Note: I'm using ST-LINK V2
2022-11-11 8:36 PM
It doesn't need an external crystal as it runs from HSI.
The BOOTx pin shouldn't make a lot of difference unless the user code sleeps the device or reconfigures pins.
More likely you're not powering it properly, issues with VDDA or VCAP
2022-11-12 2:50 AM
How stlink you use explain SWD connection show photo...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.