2020-08-18 10:01 AM
Hello,
the UART is not working.
st-link is stand alone (not connected to Nucleo anymore)
i am using a separate stm32f446ret6, tx(PIN16) and rx (PIN17) are connected to CN3 (TX/RX).
in addition the SWD CN4 of the st-link is used (all connections are made to the uC).
Programming is working fine. COM port is shown once i connect the st-link but tera term is showing nothing.
going back to a second board where the st-link is still part of the Nucleo (not break up) everything is working, uart is working.
What do you need to know to support me?
Solved! Go to Solution.
2020-08-18 11:50 AM
problem solved: i connected the tx comming from the uC to the rx of the st-link and the rx from the uC to the tx of the uC.
of course that makes sense ^^
thank you very much!!
2020-08-18 10:14 AM
Where is the ground connection? And as a test, does shorting CN3 echo the characters you type in the terminal?
2020-08-18 11:34 AM
ground is connected from CN4 (SWD) PIN 3 to ground of the uC (i think 5 times, at least 1 ground per side).
what do you mean by echo? how can i check that? i guess a multimeeter is not usable?
2020-08-18 11:40 AM
if i connect Tx and Rx on CN3 (both lines together) nothing is happening on the terminal
2020-08-18 11:50 AM
problem solved: i connected the tx comming from the uC to the rx of the st-link and the rx from the uC to the tx of the uC.
of course that makes sense ^^
thank you very much!!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.