2020-08-17 1:07 AM
I am working on NUCLEO H743ZI2 and I want to use PF0 and PF1 pins as I2C2. But on nucleo board NC is written on these pins. Can I use these pins as I2C2?
Solved! Go to Solution.
2020-08-18 3:01 AM
PF0 and PF1 are connected. Silkscreen has been updated in later revisions.
2020-08-17 1:25 AM
2020-08-17 6:22 AM
I'd be inclined to trust the board and assume those pins are not connected.
Set them up a GPIO outputs and see if you can change them, or probe directly to be certain. Schematics are also available.
2020-08-18 3:01 AM
PF0 and PF1 are connected. Silkscreen has been updated in later revisions.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.