2025-08-29 3:42 AM
I am trying to use X-CUBE-ST67W61M1 but I am failing to read any data with COM port set as document um3449 indicates (I am currently using a UART-TTL converter connected on CN7 of X-NUCLEO-ST67W61M1). I am trying to update the X-NUCLEO-ST67W61M1 firmware to see if anything changes, but NCP_update_mission_profile.bat from X-CUBE-ST67W61 does not support update with my Nucleo board. Are there any ways to bypass this problem?
Moreover, any ideas about why I am not reading anything sensible from the X-NUCLEO-ST67W61M1 UART port?
Thanks in advance for any advice
2025-09-01 10:12 AM
Hello @jacob_ ,
Have you verified the UART settings (baud rate, parity, stop bits) and ensured they match the configuration specified in the UM3449?
Serial port setting: Select COM port number, 921600 baud rate, 8-bit data, parity none, one stop bit, and
No flow control.
2025-09-02 12:39 AM
Hello @Imen.D,
Thank you for your answe first of all. The settings on my terminal are correct. In addition to this, I am not receiving anything from X-NUCLEO-ST67W61M1 when using examples of X-CUBE-ST67W61M1 (the chip does not seem to be enabled). Is UART port on CN7 still enabled for meaningful log when the board is in MISSION MODE?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.