2023-06-06 3:44 AM
i got schematics for a board that i should work on. it's stm32 L0 based.
they did put SWO also on CS of a SPI EEPROM. I'm not a hardware designer / debug protocol specialist but i could imagine debug scenarios where toggling the chip select of an EEPROM while debugging leads to unexpected results.
Would you say that putting SWO also on CS of a SPI EEPROM is safe / state of the art?
Solved! Go to Solution.
2023-06-06 5:00 AM
No problem - everyone stumbles across a misleading term or other inconsistency once in a while.
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter
2023-06-06 4:07 AM
Which STM32L0 do you have that has a SWO output?
Regards
/Peter
2023-06-06 4:43 AM
These days... they call art a rotten banana stuck on a wall. Who knows.
2023-06-06 4:51 AM
that's a good question.
they did label pb3 at the stm32l072 as SWO, as well as the pin 6 at tag connect, and then they have pb3 also labelled as cs_ee at another sheet.
after your question i looked into the l072 manual and found that it has no SWO -> the labeling is wrong.
well, I'm not a hardware designer and try to work based on the info i get
2023-06-06 5:00 AM
No problem - everyone stumbles across a misleading term or other inconsistency once in a while.
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.