2023-01-10 12:18 AM
Found this feature mentioned in Segger J-LINK wiki, but it is not clear which targets support it:
It looks like a cheap alternative of JTAG chain. From the description, I don't understand can this multidrop be done outside of a MCU chip (allows to connect several STM32s thru one ST-LINK attachment) or it refers to cores inside one MCU?
Solved! Go to Solution.
2023-01-10 1:39 AM
No, this has nothing to do with multicore, the F7 and other single cores also contain SWD protocol version 2 and can Multi-Drop. However, as far as I know, ST-LINK does not support this at present.
Regards
/Peter
2023-01-10 12:42 AM
2023-01-10 1:17 AM
So does this refer to multiple cores in a package (such as multicore H7 or wireless) or several MCUs can be connected 'passively' to one ST-LINK?
2023-01-10 1:39 AM
No, this has nothing to do with multicore, the F7 and other single cores also contain SWD protocol version 2 and can Multi-Drop. However, as far as I know, ST-LINK does not support this at present.
Regards
/Peter
2023-10-06 6:54 PM
Related https://community.st.com/t5/stm32-mcus-products/swd-multi-drop-support-on-stm32l4/m-p/80394
2023-10-08 12:22 AM - edited 2023-10-08 12:24 AM
Great. Could anybody share success story with the multi-drop? Which debug adapter (as st-links do not support it yet)?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.