2025-06-23 4:40 AM - last edited on 2025-06-23 5:00 AM by KDJEM.1
hi~!
I made a IOT prototype with STM32U031K8T6, but I can't download firmware.
The connection isn't working ad it should, can anyone tell me the issues with the attacked circuit ??
I've tried both j-link and st-link download tools.
please reply from users who have used STM32U031.
2025-06-23 4:44 AM
Welcome to the forum.
@박인구 wrote:I can't download firmware.
Please give more details - see: How to write your question to maximize your chances to find a solution
2025-06-23 5:32 AM
The schematic looks okay.
2025-06-23 5:52 AM
...except for the repeatedly inserted R7 (NRESET pull-up), which is not necessary for any STM32 because a pull-up is available internally.
However, R7 is only unnecessary and not the cause of unsuccessful downloads. As @Andrew Neil already mentioned, more information is required for this, e.g. photos of the ST-LINK used, in the case of the ST-LINK/V2 also of the back.
2025-06-23 6:01 AM
Hello,
did you have set BOOT0 pin to HIGH before you were trying to download the firmware to MCU?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-06-23 10:21 PM
Thank you for your answer. As you can see in the circuit diagram, boot0 is fixed to low.
2025-06-23 10:23 PM
Thank you for your answer. I will attach the image of the ST-Link soon.
2025-06-24 4:49 AM - edited 2025-09-25 2:37 AM
You accepted my statement as a solution.
How did you get it working?
2025-09-25 2:23 AM - last edited on 2025-09-25 2:40 AM by Peter BENSCH
Edit by ST Moderator: This post has been translated from Korean to comply with the ST Community Terms and Conditions (§10.2).
Seoul, 25 September 2025 The STM32U031K8U6 will not connect to the ST-Link SWD. Downloading is not possible.
I do not know the reason.
Have you managed to resolve this?
Debugging pins: 3.3V, SWDIO, SWCLK, NRESET, GND
NRSET is not used.
2025-09-25 2:41 AM
The same request applies to your question: more information is required for this, e.g. photos of the ST-LINK used, in the case of the ST-LINK/V2 also of the back.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.