2026-01-29 1:37 AM - last edited on 2026-01-29 1:41 AM by Andrew Neil
Does the STM32N6570-DK board support XSPI/OSPI interfaces for communication with external peripherals, or are these interfaces limited only to internal or external memory devices?
For example, if there is a Device that supports OSPI/XSPI for communication, is it possible to connect the STM32N6570-DK board to such a device to enable data exchange?
Could you please provide a clear explanation of the capabilities and practical use cases of the OSPI/XSPI interface on the STM32N6570-DK board?
Solved! Go to Solution.
2026-01-29 4:59 AM
I want to Know the Answer for ASIC thats why i had unmarked the solution and Thanks a lot for your help.
I will go through the document attached.
2026-01-29 5:00 AM
@MownishBugatha maybe PSSI helps you out? It can clock in and out 8 or 16-bits at 100 MHz.
2026-01-29 5:50 AM
ok i will check that
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.