2024-03-23 12:22 AM
i wand to work on ethernet of stm32H745i disco board , i need to generate code lwip + freertos using tool
stm32cubemx version 6.10.0 please give simple demo working project that generated by stm32cubemx version 6.10.0
or guide me how to enable lwip and freertos and ethernet driver for stm32H745i-disco board. please help me
Solved! Go to Solution.
2024-03-23 1:53 AM - edited 2024-03-23 10:22 AM
Hello,
Have a look at this link on how to create a project for STM32H7 with Ethernet and LwIP stack.
Look at this github link.
2024-03-23 1:16 AM
Hello @khodifadlalit
I suggest you to take a look at the examples using the STM32H745i-DISCO in this github repository. You can also refer to this FAQ.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-23 1:27 AM
Thanks for reply
this example code made by stmcubemx 6.9.0 tool. i use stmcubemx 6.10.0 i need to generate code using stmcubemx 6.10.0 , this possible ? i generate code stmcubemx 6.10.0 not work, please help what change required ?
2024-03-23 1:53 AM - edited 2024-03-23 10:22 AM
Hello,
Have a look at this link on how to create a project for STM32H7 with Ethernet and LwIP stack.
Look at this github link.
2024-03-23 3:00 AM
@khodifadlalit Please begin from the example advised by SofLit, exactly as is.
Do not change anything or re-generate code in "configuration tool", until you get this example working. At least, responding to ping.
2024-03-25 9:59 PM
thanks for help
above link is
example advised by SofLit, working for ping.
i generate the code using stm32cubemx version 6.10.0 and and change flash.ld file as below
/* ETH_CODE: add placement of DMA descriptors and RX buffers */
.lwip_sec (NOLOAD) :
{
. = ABSOLUTE(0x30040000);
*(.RxDecripSection)
. = ABSOLUTE(0x30040100);
*(.TxDecripSection)
. = ABSOLUTE(0x30040200);
*(.Rx_PoolSection)
} >RAM_D2
than generate code ping successfully .
than i want to move forward for send message using UDP i add
#include “lwip/udp.h” #include <string.h>
/* USER CODE BEGIN 5 */ const char* message = "Hello UDP message!\n\r"; osDelay(1000); ip_addr_t PC_IPADDR; IP_ADDR4(&PC_IPADDR, 192, 168, 1, 1); struct udp_pcb* my_udp = udp_new(); udp_connect(my_udp, &PC_IPADDR, 55151); struct pbuf* udp_buffer = NULL; /* Infinite loop */ for (;;) { osDelay(1000); /* !! PBUF_RAM is critical for correct operation !! */ udp_buffer = pbuf_alloc(PBUF_TRANSPORT, strlen(message), PBUF_RAM); if (udp_buffer != NULL) { memcpy(udp_buffer->payload, message, strlen(message)); udp_send(my_udp, udp_buffer); pbuf_free(udp_buffer); } } /* USER CODE END 5 */ but that not work
Please help ?
2024-03-26 1:45 AM
thanks for help
above link is
example advised by SofLit, working for ping.
i generate the code using stm32cubemx version 6.10.0 and and change flash.ld file as below
/* ETH_CODE: add placement of DMA descriptors and RX buffers */
.lwip_sec (NOLOAD) :
{
. = ABSOLUTE(0x30040000);
*(.RxDecripSection)
. = ABSOLUTE(0x30040100);
*(.TxDecripSection)
. = ABSOLUTE(0x30040200);
*(.Rx_PoolSection)
} >RAM_D2
than generate code ping successfully .
than i want to move forward for send message using UDP i add
Add following include files at the beginning of main.c:
#include “lwip/udp.h”
#include <string.h>
Modify the StartDefaultTask in main.c with the following code:
/* USER CODE BEGIN 5 */
const char* message = "Hello UDP message!\n\r";
osDelay(1000);
ip_addr_t PC_IPADDR;
IP_ADDR4(&PC_IPADDR, 192, 168, 1, 1);
struct udp_pcb* my_udp = udp_new();
udp_connect(my_udp, &PC_IPADDR, 55151);
struct pbuf* udp_buffer = NULL;
/* Infinite loop */
for (;;) {
osDelay(1000);
/* !! PBUF_RAM is critical for correct operation !! */
udp_buffer = pbuf_alloc(PBUF_TRANSPORT, strlen(message), PBUF_RAM);
if (udp_buffer != NULL) {
memcpy(udp_buffer->payload, message, strlen(message));
udp_send(my_udp, udp_buffer);
pbuf_free(udp_buffer);
}
}
/* USER CODE END 5 */ but that not work
Please help ?
2024-04-08 11:37 AM
Similar issue I have on the board with Mx version 6.11.0. not possible to set FREERTOS in LWIP. NO_SYS = OS Not Used. On older version the project was generated successfully. I do not know from which version it happened. After latest update I needed to config ioc file and got this issue,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.