2021-05-31 9:28 PM
Hello comrades...
I have been using IAR 6.50 for a few years now with STM32F446VC 1-- pin uC and things have been working flawlessly. I also have more recently had a project using the STM32F334 controller and debugging just fine.
Last week, all of a sudden, the Flash loading and debugging stopped working with the STM32F446. This is with the ST-Link V2 pod . I have several pods and have tried this on 3 different computers (win 10 and win 7) with the same results. It just stopped working. Compiler is fine, just the debugging and IAR interface evidently. I have not changed any software.
When I DO get IAR to connect to the target, it will sit there saying Programming Flash Memory with no progression or timeout. It does not actually erase the chip. Sometimes I get the message that there is no target device detected. This is on 3 different computers it appears.
My STM32F334 project appears to work just fine with a STM32F3 Discovery board. Need to try the actual target with the pod.
ST-Link will program the STM32F446VC from the .hex file but stopping and starting the CORE through ST-Link sometimes crashes where the STM32F334 does not crash.
I tried a new project and the full project on more than one STM32446RE-Nucleo Eval boards and I get the same results.
I also tried re-installing ST-Link drivers but nothing seems to have changed.
This really eludes me as to what might be happening. Any ideas or things to try ?
EDIT: I tried a small CubeMX program for a STM32F429ZI Discovery board and it also works fine in IAR and debugs and stops and starts etc.... It does use a different Flash EXE (.out file)
This issue must have to do with the FlashLoader software and different .OUT files that are used for flashing the parts. but I do not understand all I need to about these.
Debugging WiTHOUT download worked once on the 446 Nucleo times but otherwise says can't find the target device.
Thanks,
boB
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.