2024-03-13 10:45 AM
Hi,
I've just received a new STM32F407G-Discovery1 board from a German electronic supplier Reichelt.de.
I've connected the board with my PC (and tried also my MacBook) but the board is not recognized by the computer and doesn't power up.
A test with my ESP32 board showed that the USB port is working well.
Is there anything I could check on the board (e.g. jumper J1 is closed and if I got it right the discover jumpers are also set) or did I get a defect board.
Thanks
Bernhard
Solved! Go to Solution.
2024-03-13 11:34 AM
Hi,
thanks for the fast reply. Just figured out that I have to use the USB mini connector one the other side to get it working. What is the micro USB for?
Thanks
Bernhard
2024-03-13 11:32 AM
Hello @bkneer and welcome to the ST Community :smiling_face_with_smiling_eyes:.
I suggest you to try using a data cable (not a charging cable) and different usb port on the PC. Also, you can refer to the UM1472 for more details (specially parts 5 and 6.1).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-13 11:34 AM
Hi,
thanks for the fast reply. Just figured out that I have to use the USB mini connector one the other side to get it working. What is the micro USB for?
Thanks
Bernhard
2024-03-13 11:34 AM
Are you connecting with CN1?
Any LEDs coming on? What is LD1 doing?
2024-03-13 11:57 AM
@bkneer wrote:What is the micro USB for?
For USB OTG. The board can be used as a device and/or host. The USB mini is for the ST-Link debugger and also a power source.
2024-03-13 11:59 AM
Hi,
after I found an old mini USB cable I was able to power the board and the LEDs are on. Connecting then the micro USB I could also see the the USB is connecting.
Next step is to find out how to configure STM23CubeIDE to download a simple program. ;)
Thanks for the fast response
Bernhard
2024-03-13 12:11 PM
Hello @bkneer
You can refer to the UM2609 to understand how to use the STM32CubeIDE. If your problem is solved, close the post by choosing a best answer.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.