2025-10-28 1:37 PM
We have a custom board using STM32H750IB and a single QSPI flash memory MT25TL01G. The QSPI pin for the flash memory is the same as STM32H750B-DK board, which is PF10 for CLK, PG6 for CS, PD11/PF9/PF6/PF7 for IO0-3.
I saw several posts mentioned the external flash loader for this configuration; can anybody share the source code or the flash loader file? Thanks for the help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.