2020-02-20 12:57 AM
Hi,
i'm using CubeIDE to debug a STM32L072 micro but debug session can't be started by IDE. In the same PC i'm able to run STLink utility and STMCubeProgrammer to access SWD port properly, both of them work with same micro. I made a try with STLINK v2 and the debug session inside the IDE works fine.
The CubeIDE and ST GDB server executables are both in the whitelist of Windows Firewall.
Any suggestions?
Best regards
Giuseppe Greco
2020-02-20 12:59 AM
Sorry this is the error log:
STMicroelectronics ST-LINK GDB server. Version 5.4.0
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
ST-LINK Failed to get target status
Error in initializing ST-LINK device.
Reason: Unknown. Please check power and cabling to target.
The PC runs Windows 10
2020-02-20 4:20 AM
Generally that error indicates something basic that needs to be fixed. Do you get the same thing with another board? If not, it might be something specific to that board.
Also see if you can connect the board through STM32CubeProgrammer, as that might indicate where the problem is as well.
To get more of a clue you can also enable "Log to file" in the Debugger tab of your debug configuration and look more closely where the error happens.
2020-02-20 4:37 AM
Probably going to want to clock interface slower than 24 MHz to the L0
2020-06-15 7:00 PM
Just had exactly the same issue.
First issue was the ST-LINK GDB server "Error in initializing ST-LINK device". As soon as I checked the option to connect to a particular ST-LINK S/N and did a scan, this resolved.
Second issue was the Interface Frequency was set to Auto. Changing this to 24000 also failed. 21000 and 8000 both worked.
2020-07-27 9:16 AM
I had this issue. Turns out I was using the wrong USB cable on the G031K8. The micro USB I was using was for charging only.
2020-11-02 8:11 AM
I had the same issue with STM32L486 and CubeIDE. In other applications like ST-LINK or ST Programmer, everything is fine.
The problem is solved when I changed I/F freq. from Auto to 21000 kHz.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.