2025-11-13 8:10 AM
Hello,
I am having an issue writing the Hardware Config in the HSO Motor Pilot. I was able to do this with my previous set up, but recently upgraded from Windows 10 to Windows 11. Along with the OS upgrade, I also installed the latest releases for all the ST software so MC Workbench went from V6.3.2 to 6.4.1. I am wondering if this is a Win 11 issue or a MC Workbench issue, or possibly a debugger setting issue?
Components Used:
MC Workbench V6.4.1
STM32CubeMX V6.15.0
STM32CubeIDE V1.19.0
B-G473E-ZEST1S Control Board
STEVAL-LVLP01 Power Board
Process:
Generate project in MCWB (Sensorless HSO option) - if errors finish generating in CubeMX - Open in CubeIDE - Build / Flash with default debugger settings via USB to onboard USB STLINK - Connect to MotorPilot (Connects fine, can tune, edit values) - Select Hardware Config (either Read / Fill from UI / Import, all with same result) - Click "Write" then the board doesn't reconnect.
The errors I get in the connection bar either say "Port Open and try to configure the board" or "Port Open but no answer from board".
I have attached the log from one such session to this post.
I have not yet tried reverting to a previous version of any software yet. Would prefer to avoid that. Any help would be appreciated.
Thanks
Solved! Go to Solution.
2025-11-21 5:09 AM
Hello rms_st,
This is a known issue that will be fixed in the MCSDK's next release. In the meantime, you can change the following lines in sync_registers.c (inside):
#if defined (FLASH_OPTR_DBANK)
flashEraseInit.Page = ((uint32_t)&flashParams-FLASH_BASE) /(FLASH_PAGE_SIZE_128_BITS);
#else
flashEraseInit.Page = ((uint32_t)&flashParams-FLASH_BASE) /(FLASH_PAGE_SIZE);
#endif into :
#if defined (FLASH_OPTR_DBANK)
if (READ_BIT(FLASH->OPTR, FLASH_OPTR_DBANK) != 0U)
{
flashEraseInit.Page = ((uint32_t)&flashParams-FLASH_BASE) /(FLASH_PAGE_SIZE);
}
else
{
flashEraseInit.Page = ((uint32_t)&flashParams-FLASH_BASE) /(FLASH_PAGE_SIZE_128_BITS);
}
#else
flashEraseInit.Page = ((uint32_t)&flashParams-FLASH_BASE) /(FLASH_PAGE_SIZE);
#endifAnother solution would be to revert to MCSDK 6.3.2.
We apologise for the inconvenience.
2025-11-20 11:47 AM
Hello,
Checking if there is any update to this request.
Thanks
2025-11-21 5:09 AM
Hello rms_st,
This is a known issue that will be fixed in the MCSDK's next release. In the meantime, you can change the following lines in sync_registers.c (inside):
#if defined (FLASH_OPTR_DBANK)
flashEraseInit.Page = ((uint32_t)&flashParams-FLASH_BASE) /(FLASH_PAGE_SIZE_128_BITS);
#else
flashEraseInit.Page = ((uint32_t)&flashParams-FLASH_BASE) /(FLASH_PAGE_SIZE);
#endif into :
#if defined (FLASH_OPTR_DBANK)
if (READ_BIT(FLASH->OPTR, FLASH_OPTR_DBANK) != 0U)
{
flashEraseInit.Page = ((uint32_t)&flashParams-FLASH_BASE) /(FLASH_PAGE_SIZE);
}
else
{
flashEraseInit.Page = ((uint32_t)&flashParams-FLASH_BASE) /(FLASH_PAGE_SIZE_128_BITS);
}
#else
flashEraseInit.Page = ((uint32_t)&flashParams-FLASH_BASE) /(FLASH_PAGE_SIZE);
#endifAnother solution would be to revert to MCSDK 6.3.2.
We apologise for the inconvenience.
2025-11-21 7:47 AM
Hi Gael A,
This worked, thank you. I will keep a look out for the next release.
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.