2016-07-18 8:36 AM
One can set different frequency from Target -> Settings -> port.
Does this frequency settings effect the speed of user application or just for the speed of flash programming via SWD?And how to understand the info from ST-Link below.If you're trying to connect to a low frequency application , please select a lower SWD Frequency mode from Target->Settings menu.
In my application running at 40MHz for STM32F091, most of boards are loading Flash via SWD at 1.8M, but few had to use lower frequency to connect to target and program the flash. Does this mean those Chips using lower frequency for programming has some default?Thanks.JYI #stm32-st-link-utility-frequency2016-07-18 8:52 AM
I think low frequency in this context probably means below 1-2MHz
Do you have pull-ups on the SWDIO, SWCLK or NRST pins? If it auto-negotiates a frequency, and successfully programs, probably not a lot to worry about.2016-07-19 2:35 PM
2016-07-19 4:43 PM
Well you are going have to analyze your circuit and components as built. I'm not in a position to debug the design.
Start with voltages, look for shorts or opens. Does replacing the CPU remedy the issue?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.