2020-10-22 10:35 PM
Hi, I made a tool to flash/debug e.g. STmicro's (EBlink) that uses direct writing instead of external flash loaders. I noticed that the current speed step of the STlinkV3 goes from 8MHz directly to 24MHz with no jtag/swd speed settings in between.
Is there another API which can be used to set that speed more refined (also between 8 and 24MHz)?
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.