2020-04-27 6:28 AM
Hello,
I just bought a STLINK-V3 because of its faster USB interface to speed up debugging with STM32CubeIDE. Unfortunately I cannot get it working. With some settings the target is not found with others there are errors during flash programming. Does STM32CubeIDE support this debugger at all? If yes, is there a description how to set it up?
The STLINK-V3 works fine with STM32CubeProgrammer.
Regards
Jan
2020-04-27 7:33 AM
Hi Jan,
I think it is supported. I'm using a NUCLEO-144 board with ST-LINK v3 embedded on it and it's working fine. Check for updates of ST-LINK and STM32CubeIDE.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.