2019-10-09 4:01 PM
Pardon me if this is a red herring... the forum is hard to search.
IIRC someone (Clive?) mentioned recently that STLINK-v3 does not support connection under reset. Is it so? Then, a standalone ST-LINKv3 or built in some eval.boards?
I'm asking because going to try something on my H753 eval board that may require "hard" recovery via the debugger connection.
-- pa
2019-10-09 5:10 PM
I think I mentioned it the other day, but there was a conversation that proceeded that.
2019-10-09 5:28 PM
Yesterday
Where the commentary came from, warning from command line tool
ST-LINK Utility V4.5.0\ST-LINK_CLI.exe
[%s]: Connect under Reset is available only on ST-LINK/V2!
[%s]: Hardware Reset is available only on ST-LINK/V2!
#ElephantInTheRoom
2019-10-09 6:28 PM
Thank you.
And Keil? What says Keil debugger? I only have 5.27, not latest.
-- pa
2019-10-09 7:00 PM
Not sure, will check when I have an opportunity.
The EVAL board does have BOOT pin switches on it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.