2016-01-21 4:31 AM
Hello,
it seems that the Stlink CDC ACM implementation only sends out RX packet to the PC if the RX buffer is either full or after a delay of 100 ms. The delay when sending non-full RX packets is enourmous and slows down ''send message'' <-> ''expect response'' setups extrem. Is this delay settable somehow? E.g. the FTDI implementation exports an API to set and read this latency. #stlink #cdc-acm.-packet-latencyWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.