cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-PTOOL2V1

moh007
Associate

Hello , I want to run a BLDC motor (with hall sensors ), first I thought that STEVAL-PTOOL2V1 a plug & play control board .. I'm not a programing expert but I have a some basic knowledge .. how canI run the motor on this board ..kindly can some expliane it step by step?..

Motor parameters : is
Nominal voltage 24 V
No load speed 9960 rpm
No load current 164 mA

Nominal torque (max. continuous torque) 55.5 mNm
Nominal current (max. continuous current) 2.48 A

Terminal resistance 0.727 Ω
Terminal inductance 0.475 mH
Torque constant 22.8 mNm/A
Speed constant 418 rpm/V
Thanks in advance

0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.