2025-08-05 11:50 PM
Hi everyone, I'm having an issue with a brand new ST-Link V3 and would appreciate a quick sanity check before I return it.
Here's the situation:
* The device is not detected by my PC at all (it does not appear in Device Manager).
* I have already confirmed my USB-C data cable is working correctly.
* The red power LED on the ST-Link is extremely faint and dim.
* I also tested it on a second computer, and the result was exactly the same.
Since the LED is so dim and it fails on multiple PCs, I'm confident this is a hardware fault (DOA). Has anyone seen this specific issue before? I've attached a photo of the dim LED.
Thanks for any input!
2025-08-28 8:20 AM
Thanks @S C for the confirmation :)
Are there any plans / dates for full speed mode to be implemented in STLINK-V3? :)
This firmware is not Open-Source right?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.