2023-06-19 10:19 AM
Hello,
I was using my ST-Link/V2 ISOL, to reflash some units, but after an update with the ST link updater my programmer suddenly not recognize the target board.
I tried to reflash with different versions but it says that is corrupted. Is the ST link updater the same for all the st link programmers?
Thank you!
2023-06-19 11:22 AM
I actually have 2 other ST link V2 and the connections are exactly the same, I am able to program the boards with the other 2.
2023-06-19 3:49 PM - edited 2023-06-19 3:55 PM
Yes the st-link updater is one for all variants. Try the latest version, on a good computer (with *supported* Windows or Linux) and good cables.
Do not change other options (if shown): clock, mass storage drive, etc.
2023-06-25 9:16 AM
If the problem still exists: Can you please upload a photo of the ST-LINK/V2 ISOL and mark the faulty one there?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.