cancel
Showing results for 
Search instead for 
Did you mean: 

ST-LINK/V2-1 with V2J35M26 looses communication with MCU on Nucleo-H743ZI

ST-LINK/V2-1 with Nucleo-H743ZI loose connection when target program is run. The target program loads fine with STLINK-gdbserver coupled with gdb, but few seconds into execution, it starts to complain that it can not get status and quits after several attempts.

STMicroelectronics ST-LINK GDB server. Version 5.2.3
Copyright (c) 2019, STMicroelectronics. All rights reserved.
 
Starting server with the following options:
        Persistent Mode            : Enabled
        LogFile Name               : debug.log
        Logging Level              : 31
        Listen Port Number         : 61234
        Status Refresh Delay       : 15s
        Verbose Mode               : Disabled
        SWD Debug                  : Enabled
 
Hardware watchpoint supported by the target 
SWD frequency = 4000 kHz
ST-LINK Firmware version : V2J35S26
Device ID: 0x450
PC: 0x8040eac
ST-LINK device status: HALT_MODE
ST-LINK detects target voltage = 3.24 V
ST-LINK device status: HALT_MODE
ST-LINK device initialization OK
Waiting for debugger connection...
Waiting for connection on port 61234...
Accepted connection on port 61234...
Debugger connected
TraceCaptureStart and SWV event set to APP_TRUE 
ST-LINK device status: RESET_MODE
ST-LINK device status: RUN_MODE
ST-LINK device status: Failed to get status, Target not responding, retrying...
Target is not responding, retrying...
ST-LINK device status: Failed to get status, Target not responding, retrying...
Target is not responding, retrying...
ST-LINK device status: Failed to get status, Target not responding, retrying...
Target is not responding, retrying...
ST-LINK device status: Failed to get status, Target not responding, retrying...
Target is not responding, retrying...
ST-LINK device status: Failed to get status, Target not responding, retrying...
Target is not responding, retrying...
ST-LINK device status: Failed to get status, Target not responding, retrying...
Target is not responding, retrying...
ST-LINK device status: Failed to get status, Target not responding, retrying...
Target is not responding, retrying...
ST-LINK device status: Failed to get status, Target not responding, retrying...
Target is not responding, retrying...
ST-LINK device status: Failed to get status, Target not responding, retrying...
Target is not responding, retrying...
ST-LINK device status: Failed to get status, Target not responding, retrying...
Target is not responding, retrying...
ST-LINK device status: TMO (Max Retries)
Error! Failed to read target status 

Then, when this happens, the ST-LINK/V2-1 falls into some unknown state that STLINK-gdb complains it can not connect to the device until the ST-LINK/V2-1 is power cycled.

STMicroelectronics ST-LINK GDB server. Version 5.2.3
Copyright (c) 2019, STMicroelectronics. All rights reserved.
 
Starting server with the following options:
        Persistent Mode            : Enabled
        LogFile Name               : debug.log
        Logging Level              : 31
        Listen Port Number         : 61234
        Status Refresh Delay       : 15s
        Verbose Mode               : Disabled
        SWD Debug                  : Enabled
 
Target no device found
 
Error in initializing ST-LINK device.
Reason: No device found on target.

This issue started after upgrading to V2J35M26, so I suspect that there's a problem with this version of the firmware.

Some additional information:

  • The issue develops on two different Nucleo-H743ZI board.
  • The issue DOES NOT develop on a Nucleo-H743ZI2 (with STLINK-V3).
  • The target program runs fine on all three boards if ST-LINK/V2-1 is not controlling MCUs.

Hope someone comes up with some information about the issue (or provide a way to downgrade to older versions that I can try).

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Self resolved.

It was due to improper initialization of SWD pins.

The reason it continued to work on ZI2 board is unknown.

View solution in original post

1 REPLY 1

Self resolved.

It was due to improper initialization of SWD pins.

The reason it continued to work on ZI2 board is unknown.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.