2024-05-19 3:55 AM
Hello
I have configured TIM2 CH1 with PWM Generation on my board STM32F412G-DISCO. I capture the rising and falling edges by other board NUCLEO-G071RB, using interrupt input capture for both edges (one channel for each edge).
Now I try to change the period of the PWM in the F412G board. However, sometimes the signal stops (I capture it using an oscilloscope too).
The code I use to change the period:
fanCount=(int)(fanPeriod/1000*clock/(htim2.Init.Prescaler+1));
__HAL_TIM_SET_AUTORELOAD(&htim2,fanCount);
Do anyone have an idea what is the problem?
Solved! Go to Solution.
2024-05-19 4:31 AM - edited 2024-05-19 4:35 AM
When changing TIMx_ARR "on the fly" (without stopping the timer), you have to use ARR preload, i.e. you have to set TIMx_CR1.ARPE.
Otherwise, without preload, if you set TIMx_ARR below current TIMx_CNT, you would have to wait until TIMx_CNT rolls over the maximum, which in case of TIM2 (a 32-bit timer) is 0xFFFF'FFFF, and that can take a surprisingly long time.
(Alternatively, after setting TIMx_ARR, force update by setting TIMx_EGR.UG. Or just zero the counter, TIMx_CNT = 0.)
JW
2024-05-19 4:31 AM - edited 2024-05-19 4:35 AM
When changing TIMx_ARR "on the fly" (without stopping the timer), you have to use ARR preload, i.e. you have to set TIMx_CR1.ARPE.
Otherwise, without preload, if you set TIMx_ARR below current TIMx_CNT, you would have to wait until TIMx_CNT rolls over the maximum, which in case of TIM2 (a 32-bit timer) is 0xFFFF'FFFF, and that can take a surprisingly long time.
(Alternatively, after setting TIMx_ARR, force update by setting TIMx_EGR.UG. Or just zero the counter, TIMx_CNT = 0.)
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.