2025-08-06 7:24 AM
I am working with the NUCLEO-WL55 board and trying to generate PWM on multiple pins.
PWM output works fine on normal channels (e.g., TIM2 CH4 on PB11, TIM17 CH1 on PB9),
but I cannot get any PWM signal on TIM1 CH3N (PB15).
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_3);
HAL_TIM_PWM_Start(&htim2, TIM_CHANNEL_4);
HAL_TIM_PWM_Start(&htim17, TIM_CHANNEL_1);
__HAL_TIM_SET_COMPARE(&htim1, TIM_CHANNEL_3, 200); //ledpin pb15 ch3n
__HAL_TIM_SET_COMPARE(&htim2, TIM_CHANNEL_4, 300); //ledpin pb11 ch4
__HAL_TIM_SET_COMPARE(&htim17, TIM_CHANNEL_1, 500); //ledpin pb9 ch1
Is there a specific configuration required to enable the complementary output (CH3N) on TIM1?
Does CH3N require enabling the complementary outputs or any special polarity settings in CubeMX?
Could this be a hardware limitation of the NUCLEO-WL55 board?
Any guidance or working example for TIM1 CH3N (PB15) PWM would be appreciated.
Solved! Go to Solution.
2025-08-06 8:45 AM
Hello,
Please use the HAL_TIMEx_PWMN_Start(TIM_HandleTypeDef *htim, uint32_t Channel) function that is in stm32wlxx_hal_tim_ex.c to enable the complementary output.
2025-08-06 7:30 AM
The MOE bit needs set on advanced timers to enable output.
2025-08-06 8:45 AM
Hello,
Please use the HAL_TIMEx_PWMN_Start(TIM_HandleTypeDef *htim, uint32_t Channel) function that is in stm32wlxx_hal_tim_ex.c to enable the complementary output.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.