2021-05-04 10:57 PM
Hallo Support Team,
i have a "STEVAL-BFA001V2B" kit containing
and i had also the STEVAL-IDP004V2 master board which has a ST Link V2 programmer, is it possible to use ST Link v3 mini for programming/Debugging " STEVAL-IDP004V2" , do i need another adapter for st link V2 20 pin?.
Thanking you.
Kind Regards,
Govil
2021-05-05 9:10 AM
You'll need an adapter since the STLINK-V3MINI only has the 0.050" pitch cable connector, but the STLINK-V3MINI can be used as a programmer.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.