2020-09-16 6:40 AM
Hi, this is a newbie kind of question i think.
I have a very simple program, one that blinks a led. I can debug and run from inside STMCube IDE (all works ok), but if i upload the bin file with the STLink Utility (Windows), the program doesn't run. What i'm doing wrong?
Thanks in advance
2020-09-16 6:58 AM
Is this a custom board? What STM32 part?
Make sure BOOT0 pin is pulled low.
2020-09-16 7:48 AM
Thanks clive1 for the answer. The board is the DIYMORE STM32F407VGT6. And i was not aware of the need for pulling down BOOT0 (it seems STMCube IDE doesn't need this)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.