2019-06-06 12:38 AM
Hello!
I have installed Keil uVision and STM32 Cube on Ubuntu 18 LTE and when I try to flash the code onto my DISCO board it says that there is no board detected. I have a feel like if ST-Link2 isn't properly installed or maybe there are additional drivers for Linux that are needed in order to flash the code. I'm also running uVision via Wine. When I type usb-device on my Ubuntu terminal, the kernel sees the STM device attached to the machine via usb port.
Thank you!
2019-06-06 1:12 AM
Does the ST-Link device show up with the lsusb command ?
And, you need to grant your user access to the USB device, you might need to do this manually, i.e. add e file in /etc/udev/rules.d/.
Like here, for instance:
https://superuser.com/questions/1085991/give-application-user-access-to-usb-device
The method differs between disto families, though.
As a quick hack, you can try to run the IDE as root user. If debug access works, it is an access right issue.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.