2024-06-10 2:28 AM - edited 2024-06-10 2:37 AM
Hello,
my problem is as follows:I did a chip regression with flash erase and now I cannot connect to the mcu anymore.
I had secure area set, but I also set DMES, such that the secure area is also removed. As far as I can tell, this worked, as my secure area code had some LEDs blinking and this no longer happens.
Things I tried:
not detected (tested multiple modes to no avail)
mode: under reset, reset mode: hardware/software/core reset -> ST_Link Error: DEV_TARGET_CMD_ERR
mode: normal, reset mode: hardware reset -> ST_Link Error: DEV_TARGET_CMD_ERR
mode: normal, reset mode: software/core reset -> Error: No STM32 Target found
mode: hotplug, reset mode: hardware/software/core reset -> Error: No STM32 Target found
pulling bt0 to vdd and retrying all of the above
exactly the same results as above
flashing a piece of firmware: errors (cubeide_flash_log.txt)
debugging the firmware: errors (cubeide_debug_log.txt)
Basic command: openocd -f /usr/share/openocd/scripts/board/stm32h745i-disco.cfg -c "init"
I found some forum post that suggested setting reset_config srst_only srst_nogate connect_assert_srst. After this, openocd starts. The st link LED (COM/LD4) is flashing red and green for the first time (was only red the other times), which, according to um2408 indicates: Blinking red/green: During communication with the target
But: gdb connection dies immediately
Error: auto_probe failed
Error: Connect failed. Consider setting up a gdb-attach event for the target to prepare target for GDB connect, or use 'gdb_memory_map disable'.
setting gdb_memory_map disable helps, gdb now connects!
connecting via gdb gives me:
Error: timed out while waiting for target halted Error executing event gdb-attach on target stm32h745xih6.cpu0
gdb is there, but there is nothing meaningful I can do, reading memory always returns 0.
monitor halt times out,monitor reset gives me
monitor reset read_memory: read at 0x5c001004 with width=32 and count=1 failed Error executing event examine-end on target stm32h745xih6.cpu0: /usr/bin/../share/openocd/scripts/target/stm32h7x.cfg:237: Error: read_memory: failed to read memory in procedure 'ocd_process_reset' in procedure 'ocd_process_reset_inner' called at file "embedded:startup.tcl", line 1193 in procedure 'stm32h7x_dbgmcu_mmw' called at file "/usr/bin/../share/openocd/scripts/target/stm32h7x.cfg", line 170 in procedure 'stm32h7x_mmw' called at file "/usr/bin/../share/openocd/scripts/target/stm32h7x.cfg", line 260 in procedure 'stm32h7x_mrw' called at file "/usr/bin/../share/openocd/scripts/target/stm32h7x.cfg", line 242 at file "/usr/bin/../share/openocd/scripts/target/stm32h7x.cfg", line 237 jtag status contains invalid mode value - communication failure Polling target stm32h745xih6.cpu0 failed, trying to reexamine Examination failed, GDB will be halted. Polling again in 100ms
does not build
I am running out of ideas what is going on, how to get more info, how to debug it in general or how to fix this.
Does anyone have an idea how to fix it/how to get more information what is going on?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.