2024-07-01 8:12 AM - edited 2024-07-01 8:12 AM
I plugged in a new nucleo-h563zi, but the st-link wasn't found. The demo blinky code is running fine.
LD6 is solid green and
LD4 is slow blinking forever
On Ubuntu 22 LTS
Any ideas?
Solved! Go to Solution.
2024-07-01 8:14 AM
>>Any ideas?
Plugged into the North End USB?
Data, not charging, cable?
Drivers loading? Recognizing VID/PID for MSC, CDC/ACM and ST-LINK debugger?
2024-07-01 8:14 AM
>>Any ideas?
Plugged into the North End USB?
Data, not charging, cable?
Drivers loading? Recognizing VID/PID for MSC, CDC/ACM and ST-LINK debugger?
2024-07-01 8:23 AM - edited 2024-07-01 8:23 AM
Its the USB-C cable connected to CN1. all jumpers set to default
If I plug in the board to my PC, there is no new USB/st-link device that pops up
So no new VID/PID, pops up
2024-07-01 8:40 AM
Hello @ypearsonai
As @Tesla DeLorean suggested, try using a USB type-C Data Cable and not a charging cable that is only able to power the board, but it is not able to transfer the data from your PC to the board.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-01 8:43 AM
The cable was bad :|
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.