2023-11-16 3:08 PM - edited 2023-11-16 3:59 PM
I'm experimenting with the nucleo-h563zi board again using the examples in CubeIDE and CubeMX but I would like to end up replacing the LED/UserButton application that was originally installed when I received the board. Can't find it. Can someone point me in the right direction as to where the original firmware code or binary is located? I've submitted this question a while back and the solution was to download the original firmware binary using CubeProgrammer. Unfortunately, it's now too late for that. This is the firmware where the three LEDs flash in order and the speed of the sequence increases with each push of the User Button.
Thanks for the assist.
TJM
Solved! Go to Solution.
2023-11-17 4:53 AM
2023-11-17 4:53 AM
2023-11-17 7:28 AM
Thanks. You guys are fast.
It would be nice if they included this firmware code in the CubeH5 package. It appears there are several functions involved in this firmware that could be of interest to us while learning the board.
Thanks again,
TJM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.