Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello I am working on a group project in which we have a Nucleo-H723ZG and a CCA02M2 expansion board. We attempted to follow this quick start guide: https://www.st.com/resource/en/product_presentation/x-nucleo-cca02m2_quick_start_guide.pdf However, ...
Hii, i am new at stm32 controller & i want a pwm phase shift of 90 degree . So can anyone plz tell me that how i will generate the phase shifted pwm (what parameters we need to set to get it)
Hi All, I'm developing a project, in which I've connected the MII port of STM32F207 with Marvel IC 88E6060 (Ethernet + fiber switch) MII port 5 but the firmware support (SPL for STM32F2XX) provides libraries for DP83848 PHY only. Hence, if I...
I need development kit for STM32H725VGH6ASAP!Super ciritical
Does these boards work out of the box with an external debugger like a J-Link Ultra+? I see they both support a MIPI10 connector (and one supports a tag connector as well) that leads me to believe it supports an external debugger. However, I can't ...
Hello,I am using a H723ZG Nucleo 144 STM32 Board, with an CCA02M2 expansion mems mic board attached. I am wanting to read in audio data from the 2 built in mics on the expansion board using I2S with the nucleo board. I am unsure how to setup/configu...
Board: B-L072Z-LRWAN1MCU: STM32L072IDE: STM32CubeIDEI'm Trying to Implement RNDIS Over USB, Where When USB is Connected to Computer, It should get detected as USB Ethernet Adapter.On the STM32CubeIDE, I could Implement and Test the VCP(Virtual COM Po...
Hi, I was looking for a solution to debug STM32 microcontrollers without being physically there. I know that if I have an ST-Link connected to a PC running the GDB Server and use an IDE that supports debugging via the GDB Server, I can do so remotely...
I have a STWIN SensorTile Wireless Industrial Node development kit ( STEVAL-STWINKT1B). I try to use this code (https://github.com/STMicroelectronics/fp-sns-datalog2/tree/main/Projects/STM32L4R9ZI-STWIN/Applications/DATALOG2) on the board but the cod...
I am working with STM32H747i-DISCO discovery board, is it possible to switch between M7 and M4 core? like if I configure UART peripheral with M7 core and can I able to switch that peripheral to work with M4 core?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.