2024-11-11 2:35 AM
I am trying to put nfc02a1 with wl55jc1
I have set the settings as required in Dynamic NFC tag IC expansion board based on M24LR04E for STM32 Nucleo
But some of the pins required to be set have other functions in wl55jc1
I have reset them to match nfc02a1
But only led2 works
What is the suggested solution
Thanks in advance
Solved! Go to Solution.
2024-11-11 6:25 AM
Hello @mahmoud_zhraldeen and welcome to the ST Community.
The only solution in your case is to try to use only necessary pins of the STM32WL55JC1 for X-NUCLEO-NFC02A1. If a pin is used for another mandatory function on the NUCLEO board, you have only two solutions:
- Change it to the function needed by the X-NUCLEO-NFC02A1. In this case you can't use this pin on the previous configured function. You may can change the function to another pin if possible.
- Don't use the X-NUCLEO-NFC02A1 on this pin.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-11 6:25 AM
Hello @mahmoud_zhraldeen and welcome to the ST Community.
The only solution in your case is to try to use only necessary pins of the STM32WL55JC1 for X-NUCLEO-NFC02A1. If a pin is used for another mandatory function on the NUCLEO board, you have only two solutions:
- Change it to the function needed by the X-NUCLEO-NFC02A1. In this case you can't use this pin on the previous configured function. You may can change the function to another pin if possible.
- Don't use the X-NUCLEO-NFC02A1 on this pin.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-11 6:42 AM
Thank you for your answer
I tried to disable certain pins function in wl55jc1 by doing Reset_State and tried to turn on led but it didn't work
So I asked this question
2024-11-11 6:50 AM
If the LED pin is used for another function, you can't use it as a LED.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-11 6:52 AM
Even if I reset the state and set it as a GPIO Output??
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.