2023-05-17 3:59 AM - edited 2023-11-20 5:13 AM
new (from mouser) STLINK V3 MINIE not working on Windows PC (win7) , no driver found !
hey, on same PC STLINK V3MODS working without problem !
the brand new V3MINIE also on Win10 doing nothing - no error, no enumeration.
on win7 here :
no driver found.
and compare on USB V3mods right and V3minie left side:
different PID .
what can i do now ?
@peter BENSCH - any help ??
Solved! Go to Solution.
2023-05-23 12:51 AM - edited 2023-11-20 5:14 AM
ok, try on Win7 PC now update + change type :
..device lost. new exciting gameplay...
then:
after upgrade try plug out and in to get new enumeration, but:
then, after some minutes (!!) - working.
so:
thanks to all who have helped clarify ...
2023-05-27 10:24 AM
Have you connected the Vcc pin of MINIE to the target?
2023-05-27 10:46 AM
shure...
if you think about the 0,00V message : there was no target, just connect to St-Link was proofing connection.
problem was : need install driver (!) never need this before. new driver from STM needed.
and then update firmware / change type !
crazy...because the almost identical V3mods working instantly !
would you expect the almost same product from same company behave totally different ?
2023-05-27 12:19 PM
> would you expect the almost same product from same company behave totally different ?
These days, you know, nothing is 100% sure.
Can be bad cables, power glitches... maybe a defective or damaged st-link too.
Try to swap all parts, use a good reliable machine. Win10 or 11.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.