2022-04-30 7:52 AM
A new batch of electronic board mount an STM32F05R8T6
AA170 9U
TWN AA 131 marked.
All of this devices don't start up LSE clock.
The code is the same for about five years and makes the LSE clock start up till this days correctly. The initialization was made using example code bundled with discovery stm32F051.
I create with CubeIDE Version: 1.9.0 a minimal setup (CubeMX) for initializa internal RC but the code hangs on
while(__HAL_RCC_GET_FLAG(RCC_FLAG_LSERDY) == RESET)
{
if((HAL_GetTick() - tickstart ) > RCC_LSE_TIMEOUT_VALUE)
{
return HAL_TIMEOUT;
}
}The quartz is the same sice five years and i try to modify the capacitor from 15nF to 6,8nF with no success.
Same board with STM32F05R8T6
GQ272 9U
CHN GQ 944 marked
run perfectly.
Any ideas?
Thanks
Fabio
Solved! Go to Solution.
2023-10-09 8:14 AM
The problem seem the poor cleaning made by manufacturer when they find a Sn join between the 32Khz768 quartz pins. Fixing the unwanted join with soldering wire they don't clean well the water based flux and in some occasions made a lower impededence which makes quartz unable to run. The quartz with soldered join is covered with a 16X2 lcd display then detected dirty pin wasn't immediate.
The first batch of stm32f051RBT8 was more strong in oscillating.
Fabio
2022-04-30 8:52 AM
If you increase RCC_LSE_TIMEOUT_VALUE, does it work?
If you scope LSE, do you see a signal?
2022-04-30 9:22 AM
Doubled the value from 5000 to 10000 but nothing change...
A good board programmed with the test code for LSE created with CubeMx corectly goes over the init and chek functionality of LSE, light on a led done by a successive code..
2022-05-01 2:20 AM
> 15nF to 6,8nF
Double-check the capacitors, they surely must not be in the nF range.
Also, how exactly is VBAT connected?
Write a simple test program, which does nothing but
Note, that LSE startup times in several seconds (say up to 10s) is completely normal.
In this program, try also different RCC_BDCR.LSEDRV settings.
JW
2022-05-01 7:30 AM
Sorry my mistake, I wanted to say 15pF to 6,8pF
2022-05-01 7:54 AM
STM32F05R8T6 ?? or STM32F051R8T6 STM32F058R8T6
Can you read the device ID from the part, to be sure of the die/stepping ?
DBGMCU->IDCODE
Might need lower capacitance.
There should be a means to measure/export the LSE clock without probing directly.
2022-05-02 5:08 AM
STM32F051R8T6
AA170 9U
TWN AA 131
IDCODE 0x20006440
while(__HAL_RCC_GET_FLAG(RCC_FLAG_LSERDY) == RESET)Is the flag which manage the running/halt state ol LSE clock.
2022-05-02 5:50 AM
I mean with an oscilloscope or TIM peripheral vs HSE clock
2022-05-02 7:17 AM
@Imen DAHMEN @Amel NASRI Please check if any settings or performance changes occurred with respect to LSE clocking
The 0x2000 stepping is not covered in RM0091 Rev 9 (Jan 2017)
2022-05-02 11:04 PM
Today I tried using 3,9pF cap (the only I have in my warehouse) with no success....
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.