2023-10-09 4:13 AM
Hello,
last year I designed a prototype pcb with a F767, for programming I used the Nucleo-F767's SWD interface (with some jumpers switched), that worked perfectly.
Now I need to re-design that board, but with a H723/H733, and I just checked the Nucleo-H723 I've been working with, and I see that the ST-Link part is completely different, mostly SWD connector layout, and no more options with jumpers.
For now I would like to keep using the Nucleo-F767 including connector layout, but are there any limitations concerning MCU type or anything else?
Specifically, can I program / flash / debug a H723 with a Nucleo-F767's ST-Link?
Thanks in advance!
Solved! Go to Solution.
2023-10-09 4:56 AM - edited 2023-10-09 4:59 AM
Nucleo-H7's have ST-LINK version 3 and the "standard" mini 10-pin connector, and Nucleo F7 has ST-LINKv2. The SWD pins should be compatible. There is no good reason not to get a new ST-LINKv3 to debug your H723. This is much easier than hook a 2nd Nucleo and faster because v.3 has high-speed USB. New ST-Links v3 have 14-pin connector and cable, two extra pins on each side. The central 10 pins are same as on the 10-pin connector, two side pins are for the VCP.
2023-10-09 4:56 AM - edited 2023-10-09 4:59 AM
Nucleo-H7's have ST-LINK version 3 and the "standard" mini 10-pin connector, and Nucleo F7 has ST-LINKv2. The SWD pins should be compatible. There is no good reason not to get a new ST-LINKv3 to debug your H723. This is much easier than hook a 2nd Nucleo and faster because v.3 has high-speed USB. New ST-Links v3 have 14-pin connector and cable, two extra pins on each side. The central 10 pins are same as on the 10-pin connector, two side pins are for the VCP.
2023-10-09 4:57 AM
ST-LINK/V2 will work fine, just slower
2023-10-09 8:04 AM
Thanks, guys!
So yeah, for production later on I should directly go for the 14-pin connector, including the VCP.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.