2024-01-12 1:15 PM - edited 2024-01-12 1:17 PM
I am running macOS Sonoma and using PlatformIO within Visual Studio Code.
I have multiple STM32 microcontrollers connected via ST-LINKs to a USB hub¹. My ST-LINK USB devices are correctly listed in 1) the USB Device Tree within the macOS System Information, and 2) via Terminal when using `st-info --probe`.
I am also able to utilise these ST-LINKs to upload code to a single microcontroller individually. Even when all are connected I am able to upload code to one of these microcontrollers.
However, this happens semi-randomly. I cannot specify to which of these connected microcontrollers my code is being uploaded.
I am aware that I need a serial device address to define `upload_port` in my platformio.ini file. To find this address I am using `ls -l /dev/cu.*` in the Terminal. But the only port being returned is `/dev/cu.Bluetooth-Incoming-Port`.
Why isn’t `ls -l /dev/cu.*` showing the serial addresses of my connected ST-LINK devices? After several days of troubleshooting without any success, I would be very grateful for any insights or suggestions that could help resolve this issue!
1= Anker 4-Port Ultra-Slim USB 3.0 Hub
Solved! Go to Solution.
2024-01-14 11:36 AM - edited 2024-01-14 11:47 AM
Now without using port serials, and also thanks to the gethla tool on GitHub by a-v-s and rewriting that script to have it fully functional on macOS, I realised a different and way more simpler method:
1. Use the shell command st-info --probe to list all connected stlink programmers. When having 3 devices connected you'll see an output like the following:
Found 3 STLINK programmers
1.
version: V2J37S7
serial: 420062000E0000543233574E
flash: 524288 (pagesize: 16384)
sram: 131072
chipid: 0x0431
descr: stm32f411re
2.
version: V2J43S7
serial: 39005700180000344159544E
flash: 524288 (pagesize: 16384)
sram: 131072
chipid: 0x0431
descr: stm32f411re
3.
version: V2J43S7
serial: 18002300020000304131574E
flash: 524288 (pagesize: 16384)
sram: 131072
chipid: 0x0431
descr: stm32f411re
2. Then, integrate the device's serial number into your `platformio.ini` file using the following line:
upload_flags = -c adapter serial <serial>
3. And this made it work for me! 🥳
2024-01-12 2:54 PM - edited 2024-01-12 2:57 PM
ST-LINKs are not serial ports (though some of them contain an extra VCP function), so "cu" devices are not what you specify for tools as ST-LINK devices.
2024-01-14 11:36 AM - edited 2024-01-14 11:47 AM
Now without using port serials, and also thanks to the gethla tool on GitHub by a-v-s and rewriting that script to have it fully functional on macOS, I realised a different and way more simpler method:
1. Use the shell command st-info --probe to list all connected stlink programmers. When having 3 devices connected you'll see an output like the following:
Found 3 STLINK programmers
1.
version: V2J37S7
serial: 420062000E0000543233574E
flash: 524288 (pagesize: 16384)
sram: 131072
chipid: 0x0431
descr: stm32f411re
2.
version: V2J43S7
serial: 39005700180000344159544E
flash: 524288 (pagesize: 16384)
sram: 131072
chipid: 0x0431
descr: stm32f411re
3.
version: V2J43S7
serial: 18002300020000304131574E
flash: 524288 (pagesize: 16384)
sram: 131072
chipid: 0x0431
descr: stm32f411re
2. Then, integrate the device's serial number into your `platformio.ini` file using the following line:
upload_flags = -c adapter serial <serial>
3. And this made it work for me! 🥳
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.