2019-06-13 6:03 AM
Hi guys, I have built this STM32F334K4T6 MC dev board, I want to know if the schematic and the PCB wiring are all fine.
I also would want to know if the board will power on and will I be able to upload code to it and see an LED blink or so. I have attached the schematic and the PCB I have made. I haven't added the ground copper layer yet, its so that you can see my wiring and give it a go to send it to the fab house.
Thank you
2019-06-14 9:44 AM
But no one has told me if it works or not? will it work? can I upload code and make it do some task?
2019-06-14 10:20 AM
2019-06-14 10:24 AM
At the state it's shown, definitely no.
2019-06-14 8:10 PM
Then can you please tell me what to fix? I can send you the updated schematic I have done
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.