2025-01-09 8:11 AM
Hi,
I am currently working on a project using the NUCLEO-H755ZI-Q development board.
I am testing with a simple program that turns on the green led and goes to a while loop. I start with "full chip erase" then flash my testing program to the M7 core. I have an issue with one of my nucleo boards where it sometimes get stuck(?) during startup. When I press the reset button on the board it's 50/50 if it will boot up correctly and light up the green LED, or go into a stuck state where I can't reprogram it.
I have a second identical board to test with that doesn't have this issue. I have tried in CubeProgrammer to export all the settings from the "good" board and import them to the "bad" board, but it didn't change the behaviour.
I have also looke at the "-ob displ" output and only the serial number was different.
Any ideas of what to try next?
2025-01-09 8:32 AM
Hello,
Please check that BOOT0 pin is not floating and set to 0V.
Check these articles for common problems with STM32H7:
How to unbrick an STM32H7 after setting the wrong power mode
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.