2024-03-13 10:56 PM
How to implement I2C communication between STM32U5A9J_DK board with external LCD 16*2 I2C device
2024-03-14 12:18 AM - edited 2024-03-14 12:19 AM
Hello @ManasaPK and welcome to the ST Community :smiling_face_with_smiling_eyes:.
I don't think there is a specific Firmware for communication between STM32U5A9J_DK with LCD 16*2 External I2C device. What I suggest you is to migrate one of the available examples on the internet or YouTube using STM32F4 or other boards for examples. But why are using the external LCD 16*2? our discovery board integrate a 2.47‑inch RGB 480 × 480 pixels TFT round LCD module which you can use for a very good displaying experience:
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.