2024-02-15 11:46 PM
I was trying to drive a servo motor (MG945) from Timer 4 Channel 1 (PD12) and I succeced first time. Then I plug the cable out of my PC and change the rotation of servo motor by my bare hand. After that I pluged in cable back and then STM32F4 is gone with some burning smell :(
Now I am pluging the cable, the power LED comes on for a few seconds and then goes off again, during which time the U1 gets very hot
What should I do ? Will changing U1 fix my STM board?
2024-02-16 12:07 AM - edited 2024-02-16 12:08 AM
Hello,
It could be the regulator (U1) and or other components that gone.
Check the schematics and try to find a way to disconnect the regulator (for example remove D3) and power supply the board externally with a 3.3V source.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.