2020-04-27 2:02 AM
I have an NUCLEO-H743ZI thats works fine. So now i have buy a new NUCLEO-H743ZI2.
With the samge Firmware i not able to programming the flash.
I have upgrade the ST-Link V3 with the latest FW. But nothing helps.
When i try to programming the Flash i get follow error:
Erase Done.
Programming Done.
Contents mismatch at: 08000040H (Flash=FFH Required=C7H) !
...
Contents mismatch at: 080000E3H (Flash=FFH Required=08H) !
Too many errors to display !
Error: Flash Download failed - "Cortex-M7"
But what am I doing wrong?
Thanks for Help.
Chris
Solved! Go to Solution.
2020-04-28 5:44 AM
Thank you for your answers.
You are right, Keil uVision 5.26 does not support STLink V3.
I reinstalled Keil 5.29 and updated the ST-Link driver, now it works.
Many thanks for your help.
Chris.
2020-04-27 3:53 AM
What software you use to program? Try the latest CubeProgrammer. Check your USB cable.
-- pa
2020-04-27 4:56 AM
Thanks Pavel for your replay.
My IDE ist Keil uVison V5.26 this i use to program the Nucleo-H743ZI2.
I tried also the latest Keil V5.29. But i had the same effect.
The USB Cable ist good. I use the same to program the Nucleo-H743ZI and it works fine.
When i use the CubeProgrammer i can program the Nucleo-H743ZI2. But why not with Keil?
Chris.
2020-04-27 5:32 PM
> But why not with Keil?
So this looks like Keil issue. They have good tech. support.
-- pa
2020-04-27 6:30 PM
In Keil make sure you pick the right Flash Programming Algorithm, type of error suggests banking mode wrong/mismatched, or connection speed too high
2020-04-28 5:44 AM
Thank you for your answers.
You are right, Keil uVision 5.26 does not support STLink V3.
I reinstalled Keil 5.29 and updated the ST-Link driver, now it works.
Many thanks for your help.
Chris.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.