2021-02-06 1:12 PM
How do I connect the SWD connectors on stlink-v3 (CN6) to a stm32f104 blue pill for debugging and programming it? I am getting error "Error in initializing ST-LINK device. Reason: No device found on target." in CubeIDE 1.5.1. I want to verify my pinouts are correct and connections are correct. Any assistance would be really appreciated. I am new to this. Setting are Autostart local GDB, Debug probe = ST-LINK (ST-LINK GDB server), SWD, ST-LINK S/N was scanned and shows serial number. Enabling or disabling SWV does not fix. Type = Connect under reset.
2021-02-06 2:17 PM
The bluepill is probably not a STM32, but some clone. STLINKV3 denies connection to non-STM32 CPUs.
2021-02-08 10:21 AM
Thank you for replying Uwe, upon further checking , i have another board from same manufacturer (came from same place as I ordered two). When I connect the 2nd one, it actually connects fine and I am able to program it. I know I have used the one I am having an issue with some time ago and was able to connect to it at that time. It could be a bad board but I am doubtful this is the problem. Is there a way to reset the blue pill to allow it to connect again?
2021-02-09 12:59 AM
Connect under reset, with reset actually connected, should connect under all circumstances with an actual STM32 device.
2021-02-10 9:48 AM
Thank you. Would you be able to provide to me the actual wiring connections then between the STLink-V3 CN6 pins and the bluepill? Would that be the NRST pin needs to be connected? Sorry I am kinda new to this and trying to learn.
2021-02-10 2:43 PM
Decipher it yourself and try. if it does not work, document your findings and ask again.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.