2020-07-08 2:44 AM
During testing, Suddenly HOST PC stop detecting the board saying unknown device. NO VID/PID was recorded also. So, we need to upgrade the firmware again But the ST-Link USB is not working only. Is there any other way to upgrade it. Kindly suggest
2020-07-08 4:17 AM
Replug the device. This should bring up the bootloader. If not, you have trashed the stlink somehow. If the bootloder comes up, download stswlink-0007 and run "java -jar STLinkUpgrade.jar" in the appropriate directory.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.