2019-10-31 2:36 PM
How to fix MCO clock on NUCLEO-H743ZI2 (with MB1364C board)
Hi,
I am trying to evaluate H743ZI2, I got NUCLEO-H743ZI2.
I am trying to use HSE from MCO, but MCO clock is extremely unstable, jitter as much as 0.2%.
I verified this on 2 such boards, right from the box.
I also checked other Nucleo boards: MB1312 with L4R5ZI and MB1137 with F767ZI and they have pretty stable clock.
On MB1364C board I checked clock on:
R21 resistor - clock input to ST-Link chip - good
R5 resistor - MCO clock output from ST-Link chip - bad
SB45 - MCO - bad
So, it appears that ST-Link chip is misconfigured and generates bad clock from good.
Question: is it possible to fix it?
Thank you
2020-06-16 9:45 AM
I am using the same board and have seen a similar problem. How did you solve this? Thinking I might need to populate X3 and disconnect the MCO to the MCU.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.