2020-04-03 2:17 AM
Hello, I realised that there is less than none articles about this topic so I'm looking for advice here. Long story short, I'm trying to communicate with my Olimexino STM32 board with Virtual Com Port. I am using CubeMX to create the source code, and I'm uploding it via ST-LINK Utility with STLinkV2. I try to cummunicate with the board via RealTerm. But, everytime I load any code (even if it's just a simple blinking led) on the board it just stops showing it in the Device Manager. I tried many different ways, and I have read somwhere that it might be a wrong resistor connection problem. I am a newbie if it comes to STM32 so please be gentle. I will be very grateufl for any insight on this topic.
Cheers,
Jan
2020-04-17 9:10 AM
Hello Ons,
I did, and I have all the drivers necessary for my system installed.
I actually got my VCP working on the STM32F429-DISC1 board, but only on an example that a friend of mine provided, the examples from st.com site are still not working.
Best regards,
Jan
2020-04-17 10:42 AM
Hi Jan,
Can you please explain which example exactly that didn't work for you ?
Can you give the directory to it ?
Best Regards,
Ons.
2020-04-17 1:31 PM
> I actually have a STM32F429-DISC1 board (the one with the lcd touch-scrren) and I have tried using the CDC_Standalone projects on it too
@JWojt.1 Is this CDC_Standalone project that you have tried, been ported from other STM32F4 board?
There is no example named CDC_Standalone for STM32F429-Discovery [here]
However, this board has several USB host MSC examples.
STM32F429ZI-Nucleo has USB device examples, but not for CDC.
> I actually got my VCP working on the STM32F429-DISC1 board, but only on an example that a friend of mine provided
It's good to have friends ;) This is what ST generally advices - port an example for a similar MCU of the same family.
-- pa
2020-04-18 3:12 AM
I have tried the USB_Host example for STM32F429_DSIC1 that I downloaded from here:
https://www.st.com/en/embedded-software/stm32cubef4.html
Unfortunatley I am not looking for a host example, but for a device example.
I tried this simple tutorial, and It didn't work, the board doesn't appear in the device manager when I plug it in.
https://www.youtube.com/watch?v=7oED-m34EKk
It really got me suprised as this is one of the simplest codes I've ever seen, I have all necessary drivers installed and somehow it is still not working...
2020-04-18 6:41 AM
Perhaps it should be explained that different boards for same STM32 family have slight differences that can matter.
The board on the youtube video has STM32F407, your board has F429. These are diferent boards.
-- pa
2020-04-23 9:37 PM
Hi JWojt.1,
"There is no example named CDC_Standalone for STM32F429-Discovery [here]"
2020-05-19 3:23 AM
Hi JWojt.1,
Can we consider that this question is solved ?
Best Regards,
Ons.
2021-03-31 7:18 AM
Hi MWaqa.1,
I tried to create a HID project with Mx quickly for the STM32F429-DISC board, and I've got my device detected by Host.
Try to chose HSE Cristal/Ceramic Resonator as clock source. And share with me your .ioc file if you want.
Best Regards,
Ons.
2021-04-02 3:31 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.